cancel
Showing results for 
Search instead for 
Did you mean: 

Couldn't monitor voltage in eval l9963.

RKP.2
Associate II

Recently i bought the eval l9963 bms board from st. As i was playing with it with a 4 cell ​li-ion battery connected in series. I'm trying to monitor the battery using the STSW gui software. I connected the batteries as per the user guide connected it to co,c1,c13 and c14 respectively. Also provided the vbatt and gnd. But i'm getting the voltages abruptly. Each cell consists of 4 volts, total volt is 16. But the monitor shows only upto 11.5 volts. That too the c0 is under voltage at 2.5v ,c1 is over voltage at 5.8v,c13 is 0 and c14 is 3.6v. Could any experts guide me what i'm doing wrong here.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

Shouldn't this be in the Power Management section ?

Topic changed to Power Management and Motor Control

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RKP.2
Associate II

Can anybody guide me on this? I'm a beginner ​on the monitoring section so