2017-08-07 7:57 AM
Dear All ,
SPC5Studio 5.5.0 is available
*** Highlights ***
Here are the changes coming with SPC5Studio v5.5.0
For Mass Market:
===========-Sphaero (SPC574S) starter kit Platform component RLA Board init component RLA Basic serial RLA driver Clock component RLA IRQ Component RLA OSAL Component RLA PinMap Wizard STM, Serial, PIT and EIRQ demos- Flash driver for SPC57 family
- GTM foundation level for K2 and Lavaredo- Chorus 6M Starter Kit: - Minor bugs fixing.For Selected Customers:
================- Chorus 6M (SPC58G) starter kit Platform component RLA Board init component RLA LLD component RLA Clock component RLA IRQ Component RLA OSAL Component RLA PinMap Wizard- For Chorus 4M (SPC58EC) and 6M (SPC58G)
Ethernet, CAN and DSPI slave mode New serial driver DMA Flash driver- Power Consumption wizard
Chorus 6M (SPC58EG) support- Several bugs and improvements, please refer to
https://community.st.com/community/automotive-mcus-community/spc5-automotive-mcus/activity
(SPC5Studio part)*** Notes ***
- Make sure to read the SPC5Studio Users Guide and Components
Writers Guide in
the help section.
Enjoy SPC5Studio,
The SPC5Studio Team.
#spc58 #spc56 #spc5studio #spc572017-08-24 8:21 AM
Hello,
I have a computer can not be networked, can you provide an offline upgrade package for SPC5Studio V5.5, or update the SPC5Studio download link to the latest version (V5.0-> V5.5)?
I want to use the second CAN in Pictus,so I need at least SPC5Studio V5.3 in my offline computer.Regards
Shen
2017-08-25 3:02 AM
Hello Shen ,
Could you contact your local Field Application Engineer in China for that ?
i have not the right to provide you due to the license agreement.
for your information , i have forwarded your request to them.
Best regards
Erwan
2017-09-19 1:31 AM
Hi all.
After updating SPC5Studio to ver 5.5 I have a problem with Pin map configurations. Selection of the port and the pin are both not enabled. You can see in the pictures the previous version, and 5.5.
What could be the reason?
2017-09-19 7:22 AM
Hello Yuri ,
You should click on Advanced Mode
(Cf Screenshot)
Best regards
Erwan
2017-09-20 12:34 AM
Hi,
Erwan.
But there isn't a difference.
2018-02-10 4:49 AM
How to get SPC58EC software package?
2018-02-12 12:43 AM
hello ,
for SPC58x family ,it is for selected customers
could you send an email to
mailto:credentials@spc5studio.com
?
if the marketing guys are ok , we will send you a login/pass for spc58x support
Best regards
Erwan