2019-05-27 8:04 PM
Hi,
The demo I use is SPC560BCxx_RLA CAN Test Applicaiont
Debug LOOP Mode is OK.
In Normal Mode, when I use can_lld_transmit to send CAN messages, the status returned is always CAN_MSG_WAIT. Can you help me analyze this problem?
A preliminary confirmation is that can_lld_is_tx_empty returns FALSE causing the whole problem.
The configuration inside Demo is just to remove the FlexCAN Enable LoopBack.
Below is SFR:
Solved! Go to Solution.
2019-05-28 2:52 AM
Did you check connecting it with a CAN network? As well, if you are using a discovery board, you might need CAN transceiver in order to get CANH & CANL signals.
2019-05-28 2:52 AM
Did you check connecting it with a CAN network? As well, if you are using a discovery board, you might need CAN transceiver in order to get CANH & CANL signals.
2019-05-28 7:07 PM
ok, thanks, i will check the CAN transceiver.