2015-03-19 03:59 AM
I have configured few interrupts using Application Configuration -> ISRs (under SPC OSAL Component). I have multiple header files which I supplied to the 'Headers' parameter under 'ISRs'. I have provided 4 different header files. For another interrupt, I want one more header file. When I try to add one more file i.e. 5th one, the SPC5Studio IDE hangs (initially shows busy but later changes to 'not responding' and can not be exited). Is ther limit for no of header files for ISRs? Why is this issue?
Thanks.Mike. #interrupts---headers2015-03-30 06:22 AM
Thanks Philippe. This worked successfully although I getting some error log. Please see attached. Thanks.
Mike. ________________ Attachments : ST_SPC_ISR_Headers_plugin_error_03.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hta5&d=%2Fa%2F0X0000000aS0%2FoUQZfZ2AMOWktCHvakIvXkOQQ8s60jDXa2QweDL5mz0&asPdf=false2015-03-31 06:52 AM
Hello Mike,
the errors you mentionned are to be considered as warnings, and are not related to this topic.As soon as the version SPC5Studio3.4.3 has been delivered today (including the fixes related to this thread), let's consider this ticket as solved.Thanks and regardsPhilippe2015-03-31 10:40 PM
Thanks Philippe. Few errors have been converted to warnings but still errors are there. Not sure how harmful it is for the code. Please see attached error logs.
Thanks. Mike. ________________ Attachments : SPC_ErrorLog_v3_4_2.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hta1&d=%2Fa%2F0X0000000aRz%2FDdUvVPhtoP3Etub.UJ5OMZw.buWBSIt50KS9iJH6yx0&asPdf=falseSPC_ErrorLog_v3_4_3.log : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtYk&d=%2Fa%2F0X0000000aRl%2FTyq0EY02bKubbwDMU2JgksfmOpTvllA07D73C5H0roc&asPdf=false2015-04-01 12:17 AM
Hello Mike,
do you have any systematic step by step way of reproducing the problem ?I can see in the logs some ''Invalid Thread access'' that we did not observe on our side.RegardsPhilippe2015-04-01 05:39 AM
Hello Philippe,
I am cleaning my existing project and building it again. When I clean the project it displays these error log. Similarly, when I try to Generate Application, then also it displays the same. Other than this I am doing nothing.BTW, What is the cause for this? I haven't seen this earlier for similar actions as said above.Thanks.Mike.2015-04-02 02:22 AM
2015-04-02 10:39 PM
Hello Erwan,
Please find attached image for the below information. The language is English (US) only. No other packs installed. Thanks. Mike. ________________ Attachments : ST_SPC_ISR_Headers_plugin_error_04.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtCE&d=%2Fa%2F0X0000000aKC%2FZgrezGgVYbCRFtv8U6B1gkd2tr9qeJKNavCaPP3xyMc&asPdf=false