cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to use the debugger in Auto Dev Kit due to an expired license

ASH2930T
Associate III

Moved  from STM32 forum - this is not an STM32 question.


I am facing an issue with the Auto Dev Kit debugger. My previous license had expired (Hightec), and although I tried renewing it and even registered to get a new license, the debugger still does not work.

Additionally, I notice that the debugger and flash icons appear greyed out.

Could you please assist me in resolving this issue?

1 ACCEPTED SOLUTION

Accepted Solutions
ASH2930T
Associate III

I have solved the issue, autodevkit works with free license and the error at the start confuses you with pro that you think is not installed, but actually its the free complier which is working. So to conclude we can can just ignore the pro compiler error. 

View solution in original post

16 REPLIES 16
Ozone
Principal III

> My previous license had expired (Hightec), and although I tried renewing it and even registered to get a new license, the debugger still does not work.

This debugger licence management is fully in the hands of Hightec, nobody on this MCU forum can help with that.

They surely have a forum, helpdesk and support team as well.

ASH2930T
Associate III

Ok, but also I didn't get the answer for my 2nd question 

(Additionally, I notice that the debugger and flash icons appear greyed out.)

Could you please assist me in resolving this issue?

As you don't have a licence for the debugger, it doesn't seem unreasonable that its icons are greyed-out.

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
ASH2930T
Associate III

But I'm using the UDE starter kit 

Right, I thought that was self-explanatory.

> Could you please assist me in resolving this issue?

If you lack the experience to deal with this issue, ask your direct supervisor for assistance.

What programmer are you using? which board are you using?

I'm using this board  AEK-MCU-C4MLIT1

 

Then the UDE debugger is on board up to 256KB of code.

Just open .wsx of the project from UDE.

ASH2930T
Associate III

Yes, I did that, but it's still greyed.