2023-03-29 2:29 AM
This is the sample program I used.This is sounddb.s .
When I DEBUG a variable, I find that these pointers point to the same address.
I used two audio files. How do I have my program play the second audio file directly?I modified the userFunction as shown below.
I set the breakpoint at the location shown below.
Observe the variables as shown in the figure below.
I already extern the Engine_start1
What is the reason for this?
Solved! Go to Solution.
2023-04-03 3:08 AM
Thank you for your answer. I found the problem and solved it yesterday. The problem was with my first audio file. It ends with software information for recording audio. I recorded it using Adobe Audition. Is there any recommended audio software? Thank you for your help.
2023-03-30 7:55 AM
Hi WMa,
In the initWaveFile function the last line calls the function "checkWavFile".
This function, contained in the file sound.c., is in charge to fill the pointers to each WAV file
I hope this helps.
2023-03-30 8:21 AM
Thank you for your answer.I noticed this function. However, the values of sounddb[1].start and sounddb[0].start are the same during debugging. The correct sounddb[1].end value is not generated in this function.The whPtr parameter is still the first audio parameter.
2023-03-30 8:23 AM
The values for sounddb[1].start and sounddb[0].start are shown in the figure in my question.They're all 0x10000000.
2023-04-03 2:55 AM
Hi WMa,
I’ll check the procedure described in the UM, anyway here it is a workaround:
Step 1: Create one sounddb.s for each wave file ( see the image below)
Step 2: According to the compiler you are using, modify the file user_###.ld. adding the following code for each wave file you want load:
Step 3: In sound.c file, modify these functions: checkWavFile and initWaveFile as showed in the images below:
Step 4: In the main.c add one initWaveFile function for each wave files to play:
Step 5: modify the userFunction according to your needs.
I hope this helps.
2023-04-03 3:08 AM
Thank you for your answer. I found the problem and solved it yesterday. The problem was with my first audio file. It ends with software information for recording audio. I recorded it using Adobe Audition. Is there any recommended audio software? Thank you for your help.