2023-03-14 06:36 PM
I tried to convert audio files to HEX files,and delete all the lines in the hex file before the starting line of the audio content.Then I program the HEX file to the FLASH, but can't play. I can play with the demo program.Could you tell me how to select an audio file ? Or Provide appropriate demo audio files.
Solved! Go to Solution.
2023-03-18 12:23 PM
Dear Sir,
The file should be sampled at 44kHz stereo 32-bit samples of which first 24bits are used by the Audio Amp. The other two points to check is the volume and the starting pointer of the sound to play.
Best Regards,
AutoDevKit Team
P.S. Original sound attached.
2023-03-18 12:23 PM
2023-03-19 06:35 PM
Thank you for your answer.