cancel
Showing results for 
Search instead for 
Did you mean: 

TDA7292 with Single Supply

Alanrav
Associate

Hi, I made a circuit for the TDA7292 with a simple power supply as shown in the brochure. The standby and off functions work well, but the low tones become distorted when I increase the volume more. The circuit works with 12VDC. Is it because more DC voltage is needed? or do you have to make an additional modification to the output?

Thanks in advance.

single_tda7292.png

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
AScha.3
Chief III

Hi,

at 12V (car voltage) you can expect about 4W max.

So no "ear killer" volume possible. :)

see:

AScha3_0-1711118500719.png

So for 40W you need +/-26VDC , or 50V total.

If you feel a post has answered your question, please click "Accept as Solution".