TDA7292 with Single Supply
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-22 7:16 AM
Hi, I made a circuit for the TDA7292 with a simple power supply as shown in the brochure. The standby and off functions work well, but the low tones become distorted when I increase the volume more. The circuit works with 12VDC. Is it because more DC voltage is needed? or do you have to make an additional modification to the output?
Thanks in advance.
Labels:
- Labels:
-
Audio Amplifiers
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-03-22 7:42 AM - edited 2024-03-22 7:43 AM
Hi,
at 12V (car voltage) you can expect about 4W max.
So no "ear killer" volume possible. :)
see:
So for 40W you need +/-26VDC , or 50V total.
If you feel a post has answered your question, please click "Accept as Solution".