2016-02-29 1:26 PM
Hello,
I am testing a new STA311 design and I cannot get I2S output from the IC. I have I2S input running at 48kHz with BCK, LRCK and System clock (12.288MHz) present (coming from an ADC). I2S output is enabled but I don't have BCK or LRCK coming out.PWM output works in binary mode but I have no signal output in FFX mode. For the test, I use the APWorkbench to generate the register values and I program them via my own uC. I2C bus communication runs without errors, PWDN and RESET pins are high.Do you have any ideas what else I can try?Regards,J.2016-02-29 4:52 PM
Hi J
First , could you share your APC file , the configuration file for apworkbench , then we can understand your register setting for STA311B. and based on your description : 1) looks like volume setting is in mute status , then there are no PWM output in FFX mode , but 50% duty cycle PWM signal in binary mode . 2) if you have APWlink board , the USB interface board for ST audio device contorl by APWorkbench , you can connect I2C bus and ground to your application board , then use APworkbench to tune STA311B register setting . and for more info of APWlink , please check below link :http://www.st.com/web/en/catalog/tools/FM116/CL1620/SC1028/PF253187?s_searchtype=keyword
Thanks YT2016-03-16 9:40 AM
Thank you for the reply!
it was a cold solder joint. However, now I have I2S out only on SDO_12 and SDO_34 while I have I2S data coming to all SDIs. I also mapped all the SDOs to be the same a SDO_1 (using reg 0x37 ..0x3A) but nothing changed. Is there another register I should check, or I should suspect cold solder joint again?Regards,J.2016-03-17 10:45 AM
Hi YT,
Please find attached my test configuration file. With this file I am getting PWM on all 8 outputs but I2S only on SDO_12 and SDO_ I tested this on 4 PCBs and they all behave the same way. Regards, J ________________ Attachments : testSTA311.apc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hsz5&d=%2Fa%2F0X0000000aIF%2F6CewoWUZHMnbcJpDCf.XH3Rm2Vx2eDFE86SwDVaVYpU&asPdf=false2016-03-17 11:54 AM
its register 0x81 - SID1.
what setting in the GUI controls this?2016-03-25 12:08 AM
hi J ,
yes , the default value of 0x81 register is 0x05 hex , then SDO56 and SDO78 had been used for pop free control function. thanks YT