2021-03-25 07:36 AM
Hello,
I am using +/-40V to power TDA7293 and have no issues with its application.
I want to power an audio processor from the +40 supply rail. The audio processor needs 3.3V.
Kindly suggest a scheme to achieve this.
I am concerned about the power dissipation in the 3.3V regulator and power sequencing.
I would like to retain using the mute/stby ckt of the amplifier.
Thanks in advance!
Ravindra.
2021-03-26 03:53 AM
This will likely depend on the current that's being drawn on the 3.3v rail, which regulator you should be using:
Power sequencing is probably not needed and too expansive (to switch Vs of the amp), but you could design some circuitry to hold stby/mute low while the DCDC converter starts up.
Regards
/Peter
2021-03-26 05:37 AM
Hello,
Thank you for your early reply.
The 3.3V load can reach in the excess of 2.25W, so I was looking at L4973 and now the L4976.
I want to ensure that during power-down, the audio processor does not shut down first before the TDA7293 mutes. This along with the power dissipation of the step-down/ buck regulator is the problem I am trying to solve.
I could use L4973 (5.1V) or L4976 (5.1V) switching regulator powered from the amplifier rail and use this to power the 3.3V linear regulator with a small heat-sink. The 5V supply can also be used to power a relay (to switch the speaker) and its driver circuitry for late relay- ON and fast relay- OFF.
I need an opinion whether the above mentioned approach is any better than using an auxiliary transformer winding to generate a 5V (for relay driver circuit and relay) supply using a linear regulator. The 3.3V (audio processor) can be generated from the 5V.
Thanks!
Ravindra.