cancel
Showing results for 
Search instead for 
Did you mean: 

Please help identify this transistor, and a possible substitution. It's from a built-in phono/USB preamp from an Austrian manufactured turntable. Thanks!

J Pineda
Associate II
 
11 REPLIES 11

@Piranha​ was a bit faster than me, but we came to the same result. ��

Yes, you are right, the typo you mentioned is definitely one, and should be read a LE50ABZ-AP instead of LE33ABZ-AP. Thanks for this tip!

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
J Pineda
Associate II

Thanks @Piranha​ & @Peter BENSCH​,

Funny. I was going through that data sheet and was momentarily confused by the same typo. But...I put the LE33 on a 9v led tester and voilá, 3.3v! Out of circuit, the le33 outputs 3.36vdc. In circuit, 0.01V.

Thank you both for helping me resolve this.

Cheers,

James