2014-07-07 06:32 AM
Hello.
If I connect the board to my computer it recognizes it and installs some drivers.It will after that show up as a ''STM Device in DFU Mode'' under USB controllers in the device manager. But in the APWorkbench there is no USB port to select under the ''MEMS Microphones Demo Kit'' menu.I tried this on both windows 7 and 8 64bit.Any way I can fix this? #mki138v1-apworkbench-staudiohub2014-07-18 06:10 AM
Hi Robin,
This should not happen as it means the onboard STM32 has not been properly programmed. APW will not recognize the board as it doesn't correctly expose itself. If the problem persists please contact your local ST support or drop a private message to me. Marco2014-07-21 07:02 AM
2014-07-21 07:54 AM
Use the contact moderator feature - go back on the main page and find it on the forum's header menu.