2020-08-04 7:01 AM
LDO40L -> Enable PIN. Can I connect this pin directly to Uin to the Enabble-Pin or must I use a resistor (for example 10K for limiting Current input to the PIN Enab) to connct Enab to Uin for enable the chip?
2020-08-04 7:34 AM
The datasheet of the LDO40L allows the voltage VEN at the enable pin voltage to be in the range of -0.3V...VIN (see page 5, abs max ratings).
So connecting EN to VIN is definitely allowed, no limiting resistor is necessary.
Good luck!
/Peter
2020-08-06 11:30 PM
Thanks for your answer.
On Page 14/ figure 13
If there is an input voltage jump within 1µs, is the output voltage deviation really 2V?
Thnks an best Regards
Heiko
2020-08-06 11:59 PM
Perhaps you are referring to page 14, fig. 30 instead of fig. 13?
Then the transient at 10->15V, 1µs, Cout=2.2µF and Iout=1mA can be as high 2V, as the datasheet says. That is a typical behavior with ultra low quiescent current LDOs at low output currents and can be influenced with external circuitry.
Best regards
/Peter