cancel
Showing results for 
Search instead for 
Did you mean: 

Inputs to TDA7498/TDA7498E

DDode.2
Associate

Hi. I am planning to use TDA7498E in one of my projects and was going through the datasheet of the same and got confused at one point. In the absolute maximum ratings, it is written that the INPA, INNA, INPB, INNB have the maximum input rating of -0.3V to +4V.

The thing which got me confused is that since the analog audio signal is more or less like a sine wave with equal peaks both in positive and negative, then how are we supposed to provide the input to the TDA7498E?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Please have a look at the test circuit in the datasheet or the same schematic of the STEVAL-CCA044V1.

All of the pins you mentioned are connected to the analog input jack via a capacitor of 1µF, coupling the input AC voltage to the internal circuitry. The AC input voltage can therefore be fed in with reference to ground or with DC offset. The TDA7498E contains internal voltage dividers to provide some virtual ground behind all of these pins. The maximum input voltage of 4V then corresponds to an AC effective input voltage of 1.414V (4V/2/sqrt(2)).

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Please have a look at the test circuit in the datasheet or the same schematic of the STEVAL-CCA044V1.

All of the pins you mentioned are connected to the analog input jack via a capacitor of 1µF, coupling the input AC voltage to the internal circuitry. The AC input voltage can therefore be fed in with reference to ground or with DC offset. The TDA7498E contains internal voltage dividers to provide some virtual ground behind all of these pins. The maximum input voltage of 4V then corresponds to an AC effective input voltage of 1.414V (4V/2/sqrt(2)).

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.