2017-12-04 3:03 AM
Hi All,
I am using an SPDIF receiver, It has been connected to the STM32F401 I2S. The diagram is as bellow,
SPDIF Receiver (I2S Master) -> STM32F401 (I2S slave Receiver DMA) -> STM32F401 (DAC DMA) -> STM32F401 analog output
For a while system works perfect and I can see the analog output follows the signals which SPDIF receiver gets. But after a random amount of time which is vary from 3 minutes to 40 minutes suddenly the STM32F401's I2S DMA starts receiving wrong values.
static void MX_I2S2_Init(void)
{hi2s2.Instance = SPI2;
hi2s2.Init.Mode = I2S_MODE_SLAVE_RX; hi2s2.Init.Standard = I2S_STANDARD_MSB; hi2s2.Init.DataFormat = I2S_DATAFORMAT_16B; hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE; hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K; hi2s2.Init.CPOL = I2S_CPOL_LOW; hi2s2.Init.ClockSource = I2S_CLOCK_PLL; hi2s2.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE; if (HAL_I2S_Init(&hi2s2) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
void HAL_I2S_MspInit(I2S_HandleTypeDef* hi2s)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hi2s->Instance==SPI2) { /* USER CODE BEGIN SPI2_MspInit 0 *//* USER CODE END SPI2_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_SPI2_CLK_ENABLE(); /**I2S2 GPIO Configuration PC3 ------> I2S2_SD PB10 ------> I2S2_CK PB12 ------> I2S2_WS */ GPIO_InitStruct.Pin = GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* I2S2 DMA Init */
/* SPI2_RX Init */ hdma_spi2_rx.Instance = DMA1_Stream3; hdma_spi2_rx.Init.Channel = DMA_CHANNEL_0; hdma_spi2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_spi2_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_spi2_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_spi2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_spi2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_spi2_rx.Init.Mode = DMA_CIRCULAR; hdma_spi2_rx.Init.Priority = DMA_PRIORITY_HIGH; hdma_spi2_rx.Init.FIFOMode = DMA_FIFOMODE_DISABLE; if (HAL_DMA_Init(&hdma_spi2_rx) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(hi2s,hdmarx,hdma_spi2_rx);
/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}}
in the main() after making sure the I2S_WS is low I start the I2S DMA in the circular mode like below where
i2s_rx_buff is quite huge uint16_t type buffer
.HAL_I2S_Receive_DMA(&hi2s2, (uint16_t *)i2s_rx_buff, 3840);
The I2S receive buffer fills by half-word values as bellow, and clearly the odd index has to zero because the 16 bit out of 32 bit has been chosen. As an example the following 4 half-words has been put here where they are correct values.
0x0000-0xC4A1-0x0000-0xC493
After that unexpected events, the values shifts gradually one by one to the odd words. like bellow,
0x20FC-0x0003-0x25C0-0x0003
This bug is completely random and sometimes doesn't show even after 40-50 minutes, but sometimes it shows after a few minutes after restarting the STM32.
Some hints,
1. When I reboots the stm32 again the samples values get back to normal without bug.
2. The problem is really random and I can't see anything regular in it.
3. It seems there is something missing in i2S shift-register setting or somewhere around there.
please kindly let me know if you know what is the problem and/or you have any hint to solve it.
Thanks ~