2017-11-28 3:11 AM
Hello,
I have a question about the TS3022 dual comparators.
The datasheet states an input bias current of 300nA max. over full temperature range.
Compared to similar competitor parts this is almost two orders of magnitude higher.
I was wondering if this specification is correct or should it be pA i.s.o. nA?
Thank you,
Paul
--
2018-01-02 1:42 AM
Dear Customer,
The unit is correct. You can see the typical behavior of the IC fig 12. of the datasheet.
Best Regards,
P.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.