cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to find the part number and datasheet for ST part. 14 pin SMT device, top right corner has 324, then after the ST marking it has MZOU928. Thanks

JTauc.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

It is the LM324DT (SO14) or LM324PT (TSSOP14), both with the same marking, but you can tell them apart by the pin spacing and dimensions. Technically, they are identical.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

It is the LM324DT (SO14) or LM324PT (TSSOP14), both with the same marking, but you can tell them apart by the pin spacing and dimensions. Technically, they are identical.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JTauc.1
Associate II

Hi Peter,

Thanks for the quick reply