cancel
Showing results for 
Search instead for 
Did you mean: 

Hi,What is the input current limit through the clamp diode at TS9222 Op Amp i/p, when input exceeds the VCC- -0.3 to VCC+ +0.3 limit

HS.10
Associate
 
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
Antoine Cros
Associate II

Hello,

It is advised to limit the input current to 10mA, in order to avoid damages in the input stage of TS9222, in case the inputs exceeds the datasheet AMR conditions.

Best regards,

Antoine Cros