cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I would like to know the Power Dissipation of USBLC6-2P6 (SOT666 package). I did not find any info in the datasheet. Thanks you, G.Schaeffer

GScha.1
Associate II
 
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @GScha.1​, to the community!

The power dissipation is actually only important for TVS diodes because their test pulses last considerably longer. With ESD diodes, however, this is not important because ESD pulses are in the nanosecond range

Is there a specific reason you want the power dissipation specified?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
GScha.1
Associate II

Thanks for your answer,

I have to certify a product for ATEX (explosive atmospheres) : Thermal ignition consideration. / Directive 2014/34/EU

The temperature of a mounted component must not exceed 270°C (in case of an short-circuit for example). That is why they are looking for the power dissipation and the Rth.

Best regards,