cancel
Showing results for 
Search instead for 
Did you mean: 

Driving 2 headset in parallel with ts482idt audio amplifier

Kenny03
Associate II

Hi, 

I'm wondering if it is okay to connect 2 16ohm headsets in parallel to the ts482idt stereo amplifier. This would mean that the output load is now 8ohms but the datasheet only mentions 16 and 32 ohm loads. What if any issues would I encounter in this configuration?

 

Thanks, 

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AScha.3
Chief III

AScha3_0-1701205253223.png

at 5V:

AScha3_0-1701205475502.png

so about 80 mW in 8 ohms. you should put 8 or 10 ohms at the output, so not producing too low impedance to the amp.

why connect 2 x 16 ohm par. ?  why not connect in series ... ?

If you feel a post has answered your question, please click "Accept as Solution".
Kenny03
Associate II

since we're using a standard stereo headset here. the left and right speakers have the return lines both connected to one analog ground so it would not be possible to do a series connection. So the concern with the too low impedance is that it might pull more current than the max output spec? Our audio output is very low power (50mV and 6mA rms), so it should be okay right?

okay; if you want keep the spec , add a 10 ohm at the output, so the amp gets : 8 + 10 = 18 ohm load.

If you feel a post has answered your question, please click "Accept as Solution".