cancel
Showing results for 
Search instead for 
Did you mean: 

Configuration, set-up or help files for APWorkbench with MEMS

jmoore
Associate
Posted on September 30, 2013 at 15:53

Are there any example apc files for the MEMS microphone demonstrator? as indicated in the application note: AP4146, For example basic directional microphone set-up. There seems to be no Help available or very little supportive documentation for these boards.

1 REPLY 1
Marco VENERI
Associate II
Posted on October 01, 2013 at 09:23

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00061574.pdf

includes all relevant information about the 

http://www.st.com/web/en/catalog/tools/PF255176

board usage. Additional material is also available for each specific board which could operate with it, such as

http://www.st.com/memsmics

or the

http://www.st.com/web/en/catalog/tools/PF258331

interface.

Configuration files (.apc) can be either created by the user or provided by ST upon specific request - contact an ST representative in case of need.