cancel
Showing results for 
Search instead for 
Did you mean: 

Can't set SPIRIT1 status to lock Tx or Rx

RPink.1
Associate

I have been using STEVAL-IKR002V4D (a daughterboard with SPIRIT1 868 Mhz transceiver) to transmit data. I have it hooked with Raspberry Pi. I have followed the driver library example provided in the design kit software. However, I can't initialize the radio because it seems to stuck in the infinite loop during the VCO calibration. Upon closer examination, I found that the mc_status doesn't change after the command strobe is sent to set a status to lock TX. g_xStatus.MC_State returns 0x03 (Ready), instead of 0x0F (Lock). Do you have suggestion on how to solve this issue?

FYI, I can set it to standby, reset or ready without any problem. The problem seems to be exclusively on Lock Tx and Rx.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
0 REPLIES 0