cancel
Showing results for 
Search instead for 
Did you mean: 

Anybody knows how to measure sound intensity with microphone MAX4466?

MM.20
Associate
 
2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @MM.20​, to the community!

Well, MAX4466 is not a microphone, but a microphone preamplifier by Maxim. You must mean one of those microphone modules that are offered together with the amplifier in makershops etc, right?

There are many projects on the net that deal with this topic, e.g. this one. Most of them use a different MCU platform like e.g. Arduino, but with a little coding it should be quite easy to port it to STM32, which then offers way more performance than a small 8-bit MCU.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MM.20
Associate

0693W00000Kc0MNQAZ.pngI made a program like in the picture but it doesn't work well, it prints one value all the time. Could you help?