Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Hello,I wish to know if it possible to have references of all the boards and devices around STM32WB on this link because I wish to buy it please and the application to do work it ?https://www.youtube.com/watch?v=eqAFVi16l5EThanks a lotRegards
When Debugging the code in STM32 Cube IDE, the program execution flow directly goes into the HardFault Handler. The Debugging starts at HardFault Handler and I don't know why? Also this happened when I am trying to interface Sx1262 LoRa Module with STM32L496ZGTP. If anyone have come across similar issues please help me in this concern.Thank You
Hi,i am currently trying to read out VBAT of a STM32WB55CGU6 Board (Custom).VBAT is connected to a 3V Battery, and all other VDD pins are connected to the same battery since the board is only powered by this battery.I have setup ADC1 and enabled the VBatChannel (at least in CubeMX).My Question is how to read out the ADC Value of VBAT?So far i have tried the following: static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Common config */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.NbrOfConversion = 1; hadc1.Init.Di
Regarding the standby mode of the STM32WB5MMG, I have enabled only the RTC wake-up as trigger to wake up every second.However, occasionally it freezes in standby mode, and after a watchdog reset, it doesn't even perform initialization processes.Finally, it does not work until I manually turn the power off and on again.Do you know any workaround for this freezing issue?
When combining the standby and OTA samples (listed below), in some cases, the OTA sample is started at the timing of standby wakeup.・PWR_STANDBY_RTC・BLE_OtaIn my understand, whether the standby or OTA sample is started is determined by the first 4 bytes of SRAM1's address.Is there a case where SRAM1 becomes an undefined value in the standby, resulting in the OTA being started?
HI, I am using STM32WBA55G-DK1 board to develop ble audio device. When i call CAP_EnableAudioCodecController, it return 0x91. I have reviewed the assembly code of the project and found that CAP_EnableAudioCodecController will call hci_read_local_supported_codecs_v2 to get the codecs array. So i call hci_read_local_supported_codecs_v2 on my app code to test this api. Spoiler (Highlight to read)uint8_t num_supported_stand_codes = 0;uint8_t standard_Codec[255] = {0};uint8_t num_supported_vendor_specific_codes = 0;uint8_t vendor_specific_codes[255] = {0};status = hci_read_local_supported_codecs_v2( &num_supported_stand_codes,standard_Codec,&num_supported_vendor_specific_codes,hci_read_local_supported_codecs_v2);LOG_INFO_APP("hci_read_local_supported_codecs_v2() return status: 0x%02X\n", status);for (loop = 0; loop < num_supported_stand_codes; loop++) {LOG_INFO_APP(" %02x", standard_Codec[loop]);if (loop % 16 == 15) {LOG_INFO_APP
For our validation:I would like to verify my computation for the capacity of the bonding list size. I did have some characteristics created so it's not the default , but its a number close to that. ( Sources in the bottom) It would be disastrous if entire bonding list is cleared. (when full, and I need to prevent it )Also , I do not have the amount of devices to verify that! Please support. Pro bono publico, I also I believe you have a typo in AN5270: Here are my sources: How many keys stack can hold:https://community.st.com/t5/stm32-mcus-wireless/how-many-pairing-device-information-can-the-stm32wb-has-at-most/td-p/123506https://community.st.com/t5/stm32-mcus-wireless/storing-ble-bonding-information-keys-on-external-flash/td-p/120158How to read the actual key from stack:https://community.st.com/t5/interface-and-connectivity-ics/where-and-how-to-store-application-security-keys-on-the-bluenrg/m-p/210330What happens when stack bonding list gets full:AN5270 :
Hi everyone,I am working on the project that need to capture sound for sometime and send it to pc through BLE. I am a bit new to STM32WB,1- I have some questions regarding, how we can use on of the examples of STM32WB and turn it to this requirement.2- do we need fragmentation here? if yes what you guys suggest.Thank you.
HelloThe Nucleo/Dongle pair did not do the demo.So downloaded and updated them with P2Pserver and Client hex files.Still didn't work.Am now trying to upgrade the FUS in the dongle from .53 to current using stm32wb5x_FUS_fw_for_fus_0_5_3.bin, using 0x080EC000 as listed in Release notes, and it fails.10:39:11 : Erasing memory corresponding to segment 0:10:39:11 : Operation exceeds memory limits10:39:11 : failed to erase memoryDongle has the STM32WB55CGU6 MCU.Looks like the start address is wrong, but what should it be and where do I find this info.ThanksGiri
I am developing an application based on a STM32WB35CE and have noticed that the code generated by STM32CubeMX limits available Flash to 256k and available SRAM to 32k (the WB35CE has 512k and 96k, respectively). I have flashed the stm32wb3x_BLE_Stack_full_fw.bin copro binary, so not having all memory available is expected.according to AN5451 I should have 363k of Flash and 57k of SRAM (across the 3 SRAM banks) available for my application. How can I use these?
Hi Sir. Madam,For MB1791 Development Broad, there are 3 Type of design:MB1791-HighBand_HighPowerMB1791-HighBand_LowPowerMB1791-LowBand_HighPowerBut I doubt the BOM given, the part Description, Value and Manufacture Part Number are not tally for the Location: C8, C9, C26, C31:.Pls advise the correct value for MB1791-HighBand_HighPower.Thanks.
Hello everyone,I am working on a STM32WB5MMDK. I already posted a question about the BSP example.I have few other questions about it.I wanted to replace the Button 1 by the Button 2 so I changed it in the main file (even the CallBack). I checked the other files and the configuration was the same for the two buttons, so i didn't think i should change anything, but it doesn't work.Moreover, I also wanted to test the Humidity and Pressure Sensors (I think it is included with the Temperature Sensor since it is written as a comment), but I can't make them work (i used the same program as the one for the temperature test and just change the parameters). So, I wanted to know if someone knew how to fix those issues but mostly if there were ressources to help understand the configuration (i prefer not to use a .ioc) because i don't really find the answers to my questions online. Thank you,Nour
Hi,Many of the MuRata CMWX1ZZABZ variant support "Opne MCU" such as the -078 variant; meaning the STM32 chip is programmable. Appearently some do not have the "Open MCU" feature even though they use an STM32. Was hoping someone could clear why this is the case or at least provide which variant allow programming via ST CUBE MX etc.-Thanks
I'm new to the ST development Environment and it is my first time to be using embedded systems. My aim is to make a project of one master that communicate with multiple slaves. I have already tried the ping pong example with 2 B-L072Z-LRWAN1 boards and it works fine. my problem is that i want to assign one board to be a transmitter only and the other boards receive only. can anyone help regarding this case keeping in mind that I am new to this field.
Hi, I am new to I2S protocol, this is the first time I am working on this, I’m sorry if my question sounds trivial. I am trying to interface the RAK3172 module (STM32WLE5CC is inside) with the NAU88L25YGB audio codec from Nuvoton, the audio codec has ADCOUT and DACIN that as per the given reference design should connect to I2S_DI and I2S_DO of a MCU respectively. STM32WLE5CC/RAK3172 only has I2S2_SD pins, no separate DI and DO pins. Following is the wiring between RAK3172(STM32WLE5CC) and NAU88L25YGB. RAK3172(STM32WLE5CC) NAU88L25YGB PA3 CODEC_I2S2_MCK/MCLK PA8 CODEC_I2S2_CK/BCLK PA9 CODEC_I2S2_WS/LRCK PA10 CODEC_I2S2_SD/DI/DO (??) How can I tackle missing I2S's DI and DO pins of STM32WLE5CC? Thanks in advance for any help. -Anesh
Initially Iam flash 2 binary files to STM32WB5MMG (stm32wb5x_FUS_fw.bin & stm32wb5x_BLW_Stack_full_fw.bin ) in that case p2p Server works with ST BLE Toolbox in mobile but in my project p2p Client as another MCU.p2p Client not working well its cannot detect p2p Server and not showed in ST BLE Toolbox.I have doubt regarding p2pclient has any binary file need to flash?In my code while debug Scan_Request and Connect_Request function calls are not entered.Kindly help to guide how to work with p2p Server and p2p Client.
Hello ST Community,I am currently working with a STM32WL 55JC and I need assistance with setting the sync word for both the transmitter and receiver. Here are the details of my setup.Here I have configured my module to USE_MODEM_LORA and these are the packet params of the USE_MODEM_LORAThis below is the set sync word function whish is present in the radiodriver.c file here is the another function which is I want to use the private syncword how do i do that when i use USE_MODEM_LORA.
Hello ST experts and everyone, I am a beginner on using the STM32WLE5CC series and need some support. Currently, I have assigned to carry out verification test of STM32WLE5CC series on LORA Received Signal Strength Indicator (RSSI) and successfully set up a test system on detecting the LORA RSSI value through firmware. However, with the requirement of resource to support my test system, LORA Received Signal Strength Indicator (RSSI) accuracy (+/- ? dBm) (on receiver side) is important to verify my test system on detecting the LORA RSSI value through firmware. Therefore, I would like to ask any information or other references on it. Would apologise that I could not provide the full design of my test system due to policy and greatly appreciate to have any support or opinion on my inquiry. Thanks. Best Regards, Jack
I'm working with the WB55 Nucleo Transparent Mode projectIs there a simple way of changing the interface in an MXCUBE project from USART1 to LPUART1?
Hi Folks, I'm fancy of the STM32WL33. But it is yet not supported in the STM32CubeIDE 1.15.1. Is there an Add-On or when will it be supported? Thanks in advance
Hi,I am using BLE with FreeRTOS on STM32WB (dual core). I noticed that for BLE functionality, hw_timerserver.c is used, which is driven by the RTC timer. I have two questions about this:1) Since I am already running FreeRTOS, wouldn't it be better to replace this timerserver with osTimer - FreeRTOS timers? Or is there a specific reason why this is not a good idea?2) I am not sure how the RTC is connected with the IRQ Handler, but very often my program ends up in an unexpected interrupt area. Later, I found out it is related to the RTC_WKUP_IRQ_Handler. It seems this IRQ handler is not connected to hw_timerserver.c (I couldn't find this handler in the code, I only found HW_TS_RTC_Wakeup_Handler() and HAL_RTCEx_WakeUpTimerIRQHandler, but it seems the code never reaches these.Thank you!
Hello everyone,I am currently new to the STM32 environment. I am working with two b-L072z-LoRaWAN modules and I would like to establish peer-to-peer Lora communication between them. My goal is to configure one of the modules as a transmitter (TX) and the other as a receiver (RX) in order to send and receive messages, thus enabling a ping-pong communication between the two modules.I would like to know how I can modify the LoRa Ping pong program code tomake one module function as a master in transmitter mode and the other moduleas a slave in receiver mode.Any help or advice would be greatly appreciated.
Hi, where can I find the S2-LP chip library and examples on C. Also does STM provides any protocols with open code for frequency hopping and mesh based on sub-1 GHz external radio chip? I've found just sw package with gui to configure radio S2-LP and only for windows. I'm also happy to read any other open source solutions with frequency hopping and mesh support if you can recommend for me. Thanks in advance
Hello, I am using a P-NUCLEO STM32WB Bluetooth 5 and 802.15.4 Nucleo Pack including a USB dongle.While trying to update the FUS of the USB Dongle to set up a Thread network, I encountered several errors.Initially, I was able to connect in DFU mode, but after attempting the update, Windows no longer detected the USB dongle.I then used the ST-Link to try to perform the update, but encountered these errors:You can also find some informations related to the dongle.Is it still possible to recover the USB dongle? Any help would be appreciated,
Good morning,I am a beginner with the STM32 tools. I am working with the STM32WB5MMDK (Discovery Kit).To understand how it works, I decided to use the BSP example, but I can only see the code. I don't have a .ioc file that I could run with STM32CubeMX or STM32CubeIDE. Therefore, I don't understand how it is configured, and how the program can work without the configuration file.Does anyone know ?Thank you in advance for any help you can give me, Nour
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.