Skip to main content
Associate III
Jun 4, 2024 8:04 AM UTC
Solved

STM32WB5MMDK (Discovery Kit) - Configuration of the BSP example

Good morning,

I am a beginner with the STM32 tools. I am working with the STM32WB5MMDK (Discovery Kit).

To understand how it works, I decided to use the BSP example, but I can only see the code. I don't have a .ioc file that I could run with STM32CubeMX or STM32CubeIDE. Therefore, I don't understand how it is configured, and how the program can work without the configuration file.


Does anyone know ?


Thank you in advance for any help you can give me,

 

Nour

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 4, 2024 8:27 AM UTC

Hello @Nour 

Some of the demonstrations are elaborated without the use of CubeMX. So, there is not a .IOC file. If you want to understand, you can try other applications (that includes .ioc file) or debug this application, so you can understand how it works exactly.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 4, 2024 8:27 AM UTC

Hello @Nour 

Some of the demonstrations are elaborated without the use of CubeMX. So, there is not a .IOC file. If you want to understand, you can try other applications (that includes .ioc file) or debug this application, so you can understand how it works exactly.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NourAuthor
Associate III
Jun 4, 2024 8:47 AM UTC

Hello,

Thank you for your answer.
Do you mean that the .ioc is not available for the users, or that it was all programmed without the need to configurate the Pins of the peripherals ?

 

Best regards,

Nour

STTwo-32
ST Technical Moderator
Jun 4, 2024 8:57 AM UTC

Hello @Nour 

The pin Configurations and all other configurations are done directly on the programming tool without the generation of a .ioc file. They may be even elaborated before the CubeMX release.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.