Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
Are there any plans to add Zephyr support for the STM32WB0X line of chips? Or is it already supported with the current HAL? I couldn't find any Zephyr related information on the product page.
Hi,we are working on NOD_WL55JC for LoRaWAN network with FUOTA.we are facing problem when at the following condition1) development kit used NOD_WL55JC, firmware ( en.stm32cubewl-v1-3-0.zip) - en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA 2) device is connected to LoRaWAN 1.0.4 (OTAA) to AWS server.3) connection is successful.4) multicast setup is successful5) multicast class C is successful6) switching to class C is successful.7) fragments are received at the end device( payloads at different locations in the function ProcessRadioRxDone are debugged) while fragments are downloaded, they are not getting forwarded to the case FRAGMENTATION_DATA_FRAGMENT in LmhpFragmentationOnMcpsIndication function.can you please suggest the reason for the same or can you please share the latest firmware which is working for FUOTA example.we have attached the device log for your quick reference.thank y
Could you shed some light on what the button "start wireless stack" actually does?1) Is there some flag in flash that has to be set after flashing the wireless stack? Or is it just an option byte or something?2) Why is this seperate button necessary? It would be easier and less likely to result in long debugging sessions if flashing the stack would automatically start it as well.3) Can this process be automated via the CubeProgrammer to have a single to click to install and start wireless stack?
Hi Community,I’m trying to use the CubeMonitor-RF sniffing tool to monitor packets between my two NUCLEO-WB55 boards. I have followed all the instructions indicated by UM2288 and the ST Wiki. However, I am confused about the firmware upgrade for the M4 core using the Mac_802_15_4_Sniffer.bin file. I couldn’t find any file named Mac_802_15_4_Sniffer.bin in the en.stm32cubewb-v1-20-0 folder.Could anyone guide me on where to find this file or provide any additional steps I might have missed?Thank you!
I am using the B-L072Z-LRWAN1 and trying to optimize for low power consumption. So far I have set up the hardware by desolding SB37, SB18, R26, and D2. Now when moving JP9 from pos. 2-3 to pos. 1-2 (i.e. TCXO powered from PA12 instead of VDD_RF_LRA), I notice that the power draw changes from ~1 mA to ~3 mA. I tried disabling PA12 in CubeMX but that did not do anything.I found this solution, but i am not using any software packs other than a simple header file for the sx1276, so i can not find this mlm32l0xx_hw_conf.h file it is referring to. How else can I completely disable TCXO in the software without adding any software packs?
Hi,I'm a novice in STM32WB and BLE mesh. I have started using the "BLE_MeshLightingPRFNode" example test with the "ST BLE MESH" APP. I want to use the "vendor model" to transfer the segmented and unsegmented packets in BLE mesh network by a host node that can be a proxy node or gateway node.Although I successfully used the "ST BLE MESH" APP to communicate with the node(STM32WB5MM-DK) running "BLE_MeshLightingPRFNode" by the "vendor model". But I need to know how to use the provisioning & proxy service to communicate with mesh and its interaction.There are the questions below.In GATT "provisioning" & "proxy" services have "data in" & "data out" characteristics. I want to transmit the different data to test, trace, and check the interaction in the code. Are there guidelines about data packet format for these services and characteristics?How to transmit/receive the segmented and unsegmented data? Does BLE stack handle it? And we only need to decide the data length want to send
I want to add a new timmer application in the "BLE_MeshLightingPRFNode", so I need to know which timmer is available.Because the RTOS needs a reference timer, but I don't see the RTOS initialize and activate sequence in this sample code. Is RTOS not used in this example?And how is the "Clock configuration" in "BLE_MeshLightingPRFNode" example? Does have the cubeMX-like clock configuration diagram?
Hello I want to use PER test using Nucleo-WB55RG So, I followed the procedure in git-hub, but TX does not work. I don't know what the problem is, please help me
Hi, I have a question.I am developing a BLE HIID device using the STM32WB55 evaluation board.I am not sure how to identify multiple devices with the same firmware loaded.The problem I am currently encountering is as follows ↓↓↓.Prepare two CFG_STATIC_RANDOM_ADDRESS and switch between them on each evaluation board.Two devices appear on the advice screen (windows pairing screen)If one is connected, the other cannot be connected.I would appreciate it if you could tell me the cause of this phenomenon described above! Thank you in advance.
I am using STM32WB55 with 32 MHz HSE and am trying to find out which input clock frequency I should use for TIM16. Unfortunately it is not clear in the diagram from the datasheet. Where can I get this information? Greetings,Andreas
I have two STM32WB5MM- DK . Using an example for a diffrent board I have configured one of them as router and other as server. I dont know if they are getting connected. I need to connect these exclusively and then connect the router to Mobile phone. The major issue that I am facing is that I dont have an idea of which file should I check or update to get desired configuration.@STTwo-32
Hi, Does STM32WBA55 MCU support Bluetooth classic BR/EDR along with BLE Audio? @STTwo-32 @TDK @KDJEM.1 @IssamosThank you!
Hi I recently purchased DK board and connected to the phone to check the dumped code.But, I couldn't listen to any music nor call. I realised only few selected mobiles with BLE Audio can be used to test the board.Any solution to this? @STTwo-32 @KDJEM.1 Thanks in advance!
Hello there. I've been developing a project with STM32WLE5CCU with LoraWAN included. I've used ST's utilities like LMhandler, UTILITIES_timer, and SEQUENCER to handle tasks and different functions.I've encountered a strange behavior though. When I change the optimization level to O3 there are times where code asserts to an error and the error handler is called to reset the device.I've done some search regarding the state of the registers in the MCU and I've found out that BFSR.IMPRECISERR register was set. .... STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/MMARVALID:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/IBUSERR:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/PRECISERR:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/IMPRECISERR:0x1 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/UNSTKERR:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/STKERR:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/LSPERR:0x0 STM32WL5x_CM4/SCB/CFSR_UFSR_BFSR_MMFSR/BFARVALID:0x0 ... I've export
Iam using STM32WBA55 and i tried to configure STM32_WPAN BLE application but the generated code has a file not found error.ask me for any further details regarding this problem because i don't know what to put in my post that might help in this problem.
Hello,I want to write my own ID in the STM32WL55 memory. For this I use STM32Cubeprogram and the ST-LINK V3.My question is: is there a small flash area where I can write this identifier and which does not interfere with the code and data so as not to be deleted.I looked at the memory organization in the documentation but it's a bit confusing.Thanks.
Hi,I just have to voice my opinion on STM32's BLE STM32WB15 solution I have got, out of the box (Nucleo-WB15CC) I have spent many hours now just trying to get a simple example started just advertising to a mobile but I still can't get it too detect. Apparently reading around I have to flash "Binary" files straight to the MCU before I can get an app to work, this I just think is too much for a user (Adding that I can't seem to install STM32CubeProg). Compared to an ESP32 on espressif framework where you can get BLE up and running in a matter of minutes. I am now stuck at a stage where I have to rely on the ESP32 framework to provide a solution for my company as the STM32 equivalent is far to complexed. Add to that if this was an industrial type solution we would have to flash each MCU twice just to get them up and running! Does anyone else feel this way?
Hi, I am wondering if you can get STM32 MCU with integrated Bluetooth Classic as the only examples I have found (Like WB55) are all bluetooth low energy?
HI,I'm currently looking at the STM32WL5MOCH6STR module but I need USBC for data transfer. Any suggestion for an USBC interface chip? Thanks,
I am designing an Outdoor Radio product with STM32WLE5CBU6. my question is whether the Internal RC Oscillator is enough for my radio applications ? or do I need to add External TCXO in my circuit considering the outdoor temperature environment? for my product cost-cutting. please suggest.
I have a problem with receiving long packets (above 255 bytes) in radio FSK. Document 'an5687-longpacket-operation-with-stm32cubewl-stmicroelectronics.pdf' describes how to send and receive long packets (greater than 255 bytes). I've implemented example project 'SubGHz_Phy_Per'. I receive only errors 'OnRxError', in attachment files.I use MCU STM32WLE5CCU6 (revison Y). Is STM32WLE5CCU6 can support handling long frames (> 255 bytes)? Document wrote on page 13 "In subghz_phy_app.c, define APP_LONG_PACKET to 1 and make sure the die version is revision Y." In example project is wrote "Tx Long packet enable(payload can be greater than 255bytes. Available on stm32wl revision Y)". My MCU STM32WLE5CCU6 is from series STM32WLE.
Hello, for many years there are only 2 basic HID devices - keyboard and mouse and more recently - keyboard mouse combo! Is there any reason for not providing there examples? I guess that half of employees can do that task if this is so easy and obvious and that why it is not provided.
Hello, After prototyping with a Nucleo STM32WLJC, I start to use LoRa-E5 board from Seedstudio with a STM32WLE5 MCU.I want to make a P2P communication, so I'm trying to make a ping pong project on this board.I tried starting from seeds LoRaWan exemple, from ST pingpong exemple and also from this repo project and .ioc file(https://github.com/danak6jq/Seeed-LoRa-E5).But It's not working...After debuging I find out that in SUBGHZSPI_Transmit function, a timout error occured while waiting for TXE flag to be set.I can't find any others exemples to compare the configuration...Does anyone have a idea about whats happenning ? Or a tips that can make me move forward ? Thanks Hugo
I am trying to make communication between two Lora E5 mini modules. So, I am using SubGhz Ping pong example. I flashed program in two lora e5 modules. In one module, I am always getting HAL_SUBGHZ_ERROR_TIMEOUT in the function SUBGHZSPI_Transmit. Please help me resolve this issue.
I'm working on the STM32WL55 Nucleo-64, starting from the LoRaWAN_End_Node.I performed a hexdump and noticed that the ELF file generated at the end of the compilation process contains a significant recurrence of absolute paths, as shown in the picture below. I tried using the menu "Properties->Path and Symbols->Includes" to include all the paths through the workspace to avoid the absolute paths. What did I do wrong? How can I generate an ELF file containing only relative paths?Thank you in advance.
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.