Skip to main content
Senior
Jul 18, 2024 5:58 AM UTC
Question

BLE Router and Server

I have two STM32WB5MM- DK . Using an example for a diffrent board I have configured one of them as router and other as server. I dont know if they are getting connected.  I need to connect these exclusively and then connect the router to Mobile phone. The major issue that I am facing is that I dont have an idea of which file should I check or update to get desired configuration.

@STTwo-32 

This topic has been closed for replies.

6 replies

RiturajAuthor
Senior
Jul 23, 2024 10:48 AM UTC

I have configured one stm 32 wb as a router and another one as server . I want the router to connect to the server and then to a mobile phone to forward all the data it has recievd from server. I have been trying to figure it out but couldn't is there a way so to make sure that the stm32 get connected among themselves exclusively .

 

 

Andrew Neil
Super User
Jul 23, 2024 11:06 AM UTC

So what have you tried so far?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
RiturajAuthor
Senior
Jul 23, 2024 11:38 AM UTC

Befor this I tried to work with the mesh configuration but that did not help and is also not suitable for my application. 

I checked a document provided by ST regarding BLE and I tried to pair these by providing interrupts via push buttons but failed.

 

I have attached  both the IOC file to this