NOD_WL55JC LoRaWAN FUOTA fragments error
- 2 replies
- 1036 views
Hi,
we are working on NOD_WL55JC for LoRaWAN network with FUOTA.
we are facing problem when at the following condition
1) development kit used NOD_WL55JC, firmware ( en.stm32cubewl-v1-3-0.zip) -
en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN_FUOTA
2) device is connected to LoRaWAN 1.0.4 (OTAA) to AWS server.
3) connection is successful.
4) multicast setup is successful
5) multicast class C is successful
6) switching to class C is successful.
7) fragments are received at the end device( payloads at different locations in the function ProcessRadioRxDone are debugged)
while fragments are downloaded, they are not getting forwarded to the case FRAGMENTATION_DATA_FRAGMENT in LmhpFragmentationOnMcpsIndication function.
can you please suggest the reason for the same or can you please share the latest firmware which is working for FUOTA example.
we have attached the device log for your quick reference.
thank you in advance for your quick support.