Skip to main content
PM.5
Associate III
Aug 30, 2022 11:22 AM UTC
Solved

Dynamic display of text through USART in TOUCHGFX.

Hi...

By using Text Area widget a string is displayed on a 480x272 resolution board. But I want something like, if we give '1' from keyboard through usart that data will be transmitted & it should display a string configured in TOUCHGFX IDE .I tried it by enabling usart pins configure in polling mode & in switch case when character is received it should display a configured string .

 switch(Usart_Buffer)

  {

  case '1' :

    unicode::strncpy(textArea1Buffer,"Power on",7);

    textArea1.invalidate();

  break;

  }

I am not getting what is the proper way to do this ?

This topic has been closed for replies.
Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Sep 14, 2022 10:30 AM UTC

Hello @PM.5​ ,

I did a simple example for you on the STM32F746G-DISCO board, I will join it to this post.

To explain quickly what I did for making it work :

  • Identify which USART port you are using (can be found in the schematic file of your MCU) and provide the following parameters in CubeMX. You can choose also another Baud Rate of course. When everything is set, generate code in CubeMX.

0693W00000SvLffQAF.png

  • In TouchGFXDesigner, add a TextArea with a wildcard (and enable wildcard buffer).
  • In Model.cpp include the file "stm32xxxx_hal.h" (depending on your MCU). This file contains the reference to the "stm32xxxx_hal_uart.h" file, which implements the functions for transmitting and receiving data through the serial port.
  • Still in Model.cpp, in the tick() method, call the HAL_UART_Receive() function declared in "stm32xxxx_hal_uart.h". That will enable you, after putting it in a if statement, to detect when the serial port receives data and propagate it through the ModelListener and the ScreenPresenter for updating the UI.
void Model::tick()
{
 uint8_t pData[1] = {0};
 
 if (HAL_UART_Receive(&huart1, pData, 1, 10) == HAL_OK)
 {
 modelListener->updateCharacter(pData[0]);
 }
}
  • Create a new virtual function in ModelListener.hpp: updateCharacter(char character).
  • Then in ScreenPresenter.cpp, which inherits from the ModelListener, forward this character to the screen.
void Screen1Presenter::updateCharacter(char character)
{
 view.updateCharacter(character);
}
  • Finally, in the screen you want to display this value, create the corresponding method and copy the character in the wildcard buffer. Don't forget to invalidate the TextArea also.
void Screen1View::updateCharacter(char character)
{
 Unicode::strncpy(textArea1Buffer, &character , 1);
 textArea1.invalidate();
}

Now, if you wanna try it out, you can use a tool like Putty for simulating the UART value transmission part :

  • In the device manager, check the virtual serial port associated to your board (COM7 for me).

0693W00000SvLthQAF.png

  • In Putty, select the right COM Port and select the Baud Rate you previously chose in CubeMX.
  • Start connection and send characters into the terminal by using your keyboard.

This project could be improved, for example by using interrupts instead, but I think that might be a good start for you.

Hope that it helped,

/Yoann

Yoann KLEINST Software Developer | TouchGFX

1 reply

Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Sep 14, 2022 10:30 AM UTC

Hello @PM.5​ ,

I did a simple example for you on the STM32F746G-DISCO board, I will join it to this post.

To explain quickly what I did for making it work :

  • Identify which USART port you are using (can be found in the schematic file of your MCU) and provide the following parameters in CubeMX. You can choose also another Baud Rate of course. When everything is set, generate code in CubeMX.

0693W00000SvLffQAF.png

  • In TouchGFXDesigner, add a TextArea with a wildcard (and enable wildcard buffer).
  • In Model.cpp include the file "stm32xxxx_hal.h" (depending on your MCU). This file contains the reference to the "stm32xxxx_hal_uart.h" file, which implements the functions for transmitting and receiving data through the serial port.
  • Still in Model.cpp, in the tick() method, call the HAL_UART_Receive() function declared in "stm32xxxx_hal_uart.h". That will enable you, after putting it in a if statement, to detect when the serial port receives data and propagate it through the ModelListener and the ScreenPresenter for updating the UI.
void Model::tick()
{
 uint8_t pData[1] = {0};
 
 if (HAL_UART_Receive(&huart1, pData, 1, 10) == HAL_OK)
 {
 modelListener->updateCharacter(pData[0]);
 }
}
  • Create a new virtual function in ModelListener.hpp: updateCharacter(char character).
  • Then in ScreenPresenter.cpp, which inherits from the ModelListener, forward this character to the screen.
void Screen1Presenter::updateCharacter(char character)
{
 view.updateCharacter(character);
}
  • Finally, in the screen you want to display this value, create the corresponding method and copy the character in the wildcard buffer. Don't forget to invalidate the TextArea also.
void Screen1View::updateCharacter(char character)
{
 Unicode::strncpy(textArea1Buffer, &character , 1);
 textArea1.invalidate();
}

Now, if you wanna try it out, you can use a tool like Putty for simulating the UART value transmission part :

  • In the device manager, check the virtual serial port associated to your board (COM7 for me).

0693W00000SvLthQAF.png

  • In Putty, select the right COM Port and select the Baud Rate you previously chose in CubeMX.
  • Start connection and send characters into the terminal by using your keyboard.

This project could be improved, for example by using interrupts instead, but I think that might be a good start for you.

Hope that it helped,

/Yoann

Yoann KLEINST Software Developer | TouchGFX