Skip to main content
Associate III
May 25, 2022
Question

Hello,I have a project with an 800x480 touch screen, 1 Go Ram, 2 Go Nand and 2 Go µSD, I can use the STM32MP1xx but I don't know Linux, is there an equivalent component in the STM32F7xx series?Best regards

..

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
May 25, 2022

This is essentially the same question you have already asked here.

The STM32MP1 as a CPU is perfectly designed to work with external flash and external RAM, whereas with the same structure you don't really use the full potential of the Cortex-M. Microcontrollers with Cortex-M cores are optimised for maximum processing speed using internal memory. 

For your purposes, you could look at one of the many DISCOVERY boards, e.g. the STM32H745I-DISCO, whose design still needs to be adapted to your needs (WVGA, much more memory).

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
May 25, 2022

You'll need to get your RAM footprint down significantly to entertain an F7 or H7.

Perhaps time to learn how to Linux..​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Super User
May 25, 2022

All you've told us is what storage & display your system has - nothing about what the system needs to do.

Does it actually need all those memories at those sizes?

Impossible to say what might be appropriate with no idea of what the goal is!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.