Skip to main content
Jliu.21
Associate
January 30, 2021
Question

STM32MP157 mdio can not get ethernet phy

  • January 30, 2021
  • 2 replies
  • 1818 views

the kernel log is : mdio_bus stmmac-0: MDIO device at address 7 is missing.

phy chip is : ksz9031

mpu is : stm32mp157cac3

my dts config is :

&ethernet0 { status = "okay"; pinctrl-0 = <&ethernet0_rgmii_pins_a>; pinctrl-1 = <&ethernet0_rgmii_pins_sleep_a>; pinctrl-names = "default", "sleep"; clock-names = "stmmaceth", "mac-clk-tx", "mac-clk-rx", "ethstp", "eth-ck"; clocks = <&rcc ETHMAC>, <&rcc ETHTX>, <&rcc ETHRX>, <&rcc ETHSTP>, <&rcc ETHCK_K>; assigned-clocks = <&rcc ETHCK_K>; assigned-clock-parents = <&rcc PLL4_P>; assigned-clock-rates = <125000000>; phy-mode = "rgmii"; max-speed = <1000>; phy-handle = <&phy0>; st,eth_clk_sel; mdio0 { #address-cells = <1>; #size-cells = <0>; compatible = "snps,dwmac-mdio"; reset-gpios = <&gpiog 0 GPIO_ACTIVE_LOW>;phy0: ethernet-phy@7 { reg = <7>; /* * These skews assume the STM32MP1 has no internal delay. * * All skews are offset since hardware skew values for the ksz9031 * range from a negative skew to a positive skew. * See the micrel-ksz90x1.txt Documentation file for details. */ /* REG 0x0008, 5 bits per skew */ txc-skew-ps = <1800>;/* 900ps */ rxc-skew-ps = <1320>;/* 420ps */ /* REG 0x0004, 4 bits per skew */ txen-skew-ps = <420>; /* 0ps */ rxdv-skew-ps = <420>; /* 0ps */ /* REG 0x0005, 4 bits per skew */ rxd0-skew-ps = <720>; /* 300ps */ rxd1-skew-ps = <780>; /* 360ps */ rxd2-skew-ps = <840>; /* 420ps */ rxd3-skew-ps = <900>; /* 480ps */ /* REG 0x0006, 4 bits per skew */ txd0-skew-ps = <0>; /* -420ps */ txd1-skew-ps = <60>; /* -360ps */ txd2-skew-ps = <120>; /* -300ps */ txd3-skew-ps = <180>; /* -240ps */ micrel,force-master; }; };};

the dts config is copied from a runnable dts config which is using a linux4.19 ,but my ver is 5.4

This topic has been closed for replies.

2 replies

allard
Senior
February 1, 2021

Is the PHY configured for address 7?

Jliu.21
Jliu.21Author
Associate
February 1, 2021

Yes. I got the adress from another dts which makes it work well. But the version of that kernel is 4.x

OlivierK
ST Technical Moderator
February 1, 2021

​Hi Jliu.2 (Community Member)

I suggest to not to mix kernel versions since you will face lots of potential issues. (TFA/U-boot/Kernel+DT) should be homogenous from the same OpenSTLinux version.

The DT you describe here doesn't tell anything strange. MDIO device at address 7 can be seen in kernel 5.4 version also.

Regards,

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.