Skip to main content
FHopp.1
Associate III
December 16, 2020
Solved

STM32L476RGT which are the 5V tolerant pins? Where can I find these infomation in data sheet?

  • December 16, 2020
  • 1 reply
  • 2016 views

Hello, I use for STM32 (1.8V VDD) SPI communication with an slave temperature Sensor (3.5V basic voltage, detects high at 0,7*3,5V)

SCLK =PC10

SDO = PC11

SDI= PC12

CS = PC13

For that reason I want to use an external 3.5V Pullup. But I'm not sure if this is OK for pins

PC10/PC11/PC12/PC13. Can anybody tell me if this is OK?And where I can find these information in datasheet? I already looked in the AN4899 Application note, but coulkdn't find which pins are 5V tolerant. In special if PC10/11/12/13 are 5V tolerant.

Best regards

Fabian

This topic has been closed for replies.
Best answer by Imen.D

Hello @FHopp.1​ 

You can refer to the STM32L476xx datasheet, and see the tables:

  • Table 15: Legend/abbreviations used in the pinout table 
  • Table 16: STM32L476xx pin definitions table 0693W000006G18vQAC.png

Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.

Imen

1 reply

Imen.DBest answer
ST Technical Moderator
December 16, 2020

Hello @FHopp.1​ 

You can refer to the STM32L476xx datasheet, and see the tables:

  • Table 15: Legend/abbreviations used in the pinout table 
  • Table 16: STM32L476xx pin definitions table 0693W000006G18vQAC.png

Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks