cancel
Showing results for 
Search instead for 
Did you mean: 

How to check whether the SPC560B54L5 EVB IS IN STANDBY mode or not?

rpoon
Associate II

0693W000000U6AvQAK.jpgHello,

I am trying to make SPC560B54L5 EVB in low power mode that is STANDBY mode.

The measured current in normal RUN0 mode is 143 mA whereas while keeping in STANDBY mode, it is around 92 mA. But as per the AN3316 Application note the max current consumption is 314uA. So am I entering into STANDBY mode correctly?

Because I could see that USB is getting disconnected during waiting for the S_MTRANS to SET.

 while (ME.IS.R == 0U){

  ;

 }

How can I make sure rather SPC560B54L5 EVB is in standby mode or not?

BEST REGARDS

Rewatee

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello Rewatee ,

Maybe you have some measurement issues

I am not an expert to measure a MCU in low power mode

There is a nice example in the application wizard

SPC560Dxx_RLA WKPU API Test Application for Discovery

The core should display Core Inactive on a debug session

Best Regards

Erwan

0693W000000U7QBQA0.png

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Hello Rewatee ,

Maybe you have some measurement issues

I am not an expert to measure a MCU in low power mode

There is a nice example in the application wizard

SPC560Dxx_RLA WKPU API Test Application for Discovery

The core should display Core Inactive on a debug session

Best Regards

Erwan

0693W000000U7QBQA0.png