Skip to main content
SwineOne
Associate II
October 14, 2019
Solved

[Bug Report + Fix] HAL I2C interrupt handler not working

  • October 14, 2019
  • 3 replies
  • 2652 views

While writing the simplest example I could come up for using the HAL I2C routines, I came across what seems like a clear-cut bug. This is for the latest version of STM32CubeF4 (1.24.0), identified in stm32f4xx_hal.c as "STM32F4xx HAL Driver version number V1.7.5".

To be clear, I only want to write some data to an I2C device using HAL_I2C_Master_Transmit_IT(). I configured the I2Cx EV interrupt and I2Cx_EV_IRQHandler() simply calls HAL_I2C_EV_IRQHandler(), passing in the proper I2C handle.

Running the code with a logic analyzer hooked up, I notice only the slave address is sent. After that, SCL is pulled low indefinitely, the next bytes aren't transmitted, and the I2C stop signal isn't sent.

Debugging the code shows that the code is stuck rerunning HAL_I2C_EV_IRQHandler() endlessly -- just as it leaves the ISR, it immediately comes back there.

Cutting the story short, here is the issue:

In the I2C_Master_SB() function (inside the file stm32f4xx_hal_i2c.c, line 5452), there is the following check:

      if ((hi2c->hdmatx->XferCpltCallback != NULL) || (hi2c->hdmarx->XferCpltCallback != NULL))

      {

        /* Enable DMA Request */

        SET_BIT(hi2c->Instance->CR2, I2C_CR2_DMAEN);

      }

In my case, since I'm using interrupts and not DMA, it follows that both hdmatx and hdmarx are NULL. However, numerically NULL equals 0, which is a valid memory address, and contains the interrupt vector. Therefore, the access to hi2c->hdmatx or hi2c->hdmarx is a valid memory access which, given the struct offset of the XferCpltCallback field, corresponds to the SysTick handler, which isn't NULL. So, the DMAEN bit gets inadvertently set.

Back in the HAL_I2C_EV_IRQHandler() (line 4568 of stm32f4xx_hal_i2c.c), we have the following code:

    /* I2C in mode Transmitter -----------------------------------------------*/

    else if (I2C_CHECK_FLAG(sr2itflags, I2C_FLAG_TRA) != RESET)

    {

      /* Do not check buffer and BTF flag if a Xfer DMA is on going */

      if (READ_BIT(hi2c->Instance->CR2, I2C_CR2_DMAEN) != I2C_CR2_DMAEN)

      {

        ...

      }

The code inside (which I replaced by ...) is what needs to run for the transmission to occur. However, because DMAEN was previously set, the if() condition is false and the code inside never runs.

In my opinion, the fix is to check if hi2c->hdmatx and hi2c->hdmarx are not NULL prior to checking if the callbacks are NULL. Concretely, replacing line 5452 with the following solves the issue, which I propose as a fix:

    if ((hi2c->hdmatx != NULL && hi2c->hdmatx->XferCpltCallback != NULL) || (hi2c->hdmarx != NULL && hi2c->hdmarx->XferCpltCallback != NULL))

This topic has been closed for replies.
Best answer by Mike_ST

Hello,

Please check HAL F4 v1.24.1:

  • HAL I2C update
  • Fix I2C send break issue in IT processes
    • Add additional check on hi2c->hdmatxand hi2c->hdmarx to avoid the DMA request enable when ITmode is used.

3 replies

Mike_ST
Mike_STBest answer
ST Technical Moderator
October 14, 2019

Hello,

Please check HAL F4 v1.24.1:

  • HAL I2C update
  • Fix I2C send break issue in IT processes
    • Add additional check on hi2c->hdmatxand hi2c->hdmarx to avoid the DMA request enable when ITmode is used.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
SwineOne
SwineOneAuthor
Associate II
October 14, 2019

Thanks, my bad. My development environment hasn't been updated to CubeF4 v1.24.1 yet, so this is why I wasn't seeing the fix.

Mike_ST
ST Technical Moderator
October 14, 2019

No problem :)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.