Skip to main content
BCowa
Associate
August 23, 2019
Question

Normal files needed to use STM8 with STVD and Cosmic

  • August 23, 2019
  • 0 replies
  • 1024 views

I am working on my first STM8 project and getting used to its own flavour of quirks etc.

Setting up a new project installs stm8s_interrupt_vector.c which I understand. I want to use the standard peripheral drivers so have downloaded them and added the .c and .h files to my project code files.

I now cannot find stm8s_it.h or .c from the latest software download. Is there any reason they have disappeared? I assume i need them because all the stm8s cosmic tutorials always include them.

Lastly I have found iostm8.h which appears to define the cpu registers if I want to access them without using the main peripheral drivers. Is that correct? and if so am I correct in assuming I do not need this file it I am using the peripheral drivers.

A quick clarification on these files would be agreat help please guys.

Cheers, Bruce

    This topic has been closed for replies.