cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN240 - never get fault interrupt

TLjub
Associate

I'm driving a small engine and almost everything works well. Running current is about 13mA and 80mA at the end when it is directly driven. When driving with the STSPIN240 and the actuator come to an end the driver's output go into switch mode and limit current by Vref. But the Fault pin never change the state what I need to detect the end. I have tried the values of the components from the datasheet and also with different values the result is the same. What do I do wrong or do I expect wrong?

0 REPLIES 0