I2C pcb and pull-up
Good morning, I wanted to ask a question about the I2C interface.
In particular on the routing of the pcb, I have a micro STM32 that is the master for i2c bus, then there are 2 slaves on the board and a connector to allow the connect of a third.
The question is: the SDA and SCL tracks must all start from the STM32 and go to each slave or from the STM32 I have to go to the first slave, then from this to the second slave and so on.
and in both cases, pull-up resistances where they must be positioned? can I use the STM32 internal pull-ups?
thansk in advance