cancel
Showing results for 
Search instead for 
Did you mean: 

I-NUCLEO-LRWAN1 compatible boards?

bdaniel7
Associate II

Hi,

I have two boards that I would like to use with the I-NUCLEO-LRWAN1 expansion board:

NUCLEO-F411RE and NUCLEO-L152RE.

Is any of them compatible with I-NUCLEO-LRWAN1?

Thanks.

4 REPLIES 4
Imen.D
ST Employee

Hello @DB.7lendea​ ,

Yes, these boards are compatible with  I-NUCLEO-LRWAN1.

You can check the compatible products and softwares on the board page:

https://www.st.com/en/evaluation-tools/nucleo-f411re.html

https://www.st.com/en/evaluation-tools/nucleo-l152re.html

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

You're talking through the USART on D0/D1 of the shield, I don't think NUCLEO-64 boards are ideal for that as you have some clashing with the VCP, but you should be able to resolve with SB (solder bridges) changes.

The NUCLEO-144 or DISCO boards with shield would be arguably better choices.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
bdaniel7
Associate II

Ok, noted.

Thanks.

bdaniel7
Associate II

Hmm,

I see in the technical documentation for the I-CUBE-LRWAN software, only the following boards are supported:

NUCLEO-L053R8

NUCLEO-L073RZ

NUCLEO-L152RE

NUCLEO-L476RG

Do I need to make some changes in the software to be able to use the F411RE board?