cancel
Showing results for 
Search instead for 
Did you mean: 

ST MC Workbench + ST FOC library

m239955_stm1
Associate
Posted on July 14, 2013 at 01:39

Hi, as I couldn´t get any ifn003v1 board, I bought an EVAL6230QR with an stm32f4discovery, and I´m trying to get them work together with the ST FOC library the ST MC Workbench and a MAXXON motor (EC-max 283833).

I´m trying to run the demo code, the one that starts and stops the motor repeatedly. But it turns out that it resets because of a fault. by debugging I could find that the error is defined as MC_SPEED_FDBK, and I was trying to find out why.

Is the St MC workbench set wrong? I´m wiring something wrong? I will appreciate any help to set the parameters correctly.

Thanks in advance,

Best Regards

1 REPLY 1
Gigi
ST Employee
Posted on July 15, 2013 at 09:35

Ciao

Please take a look at [DEAD LINK /public/STe2ecommunities/motordriver_ics/Lists/Motor%20Control%20Firmware%20and%20Software/Flat.aspx?RootFolder=/public/STe2ecommunities/motordriver_ics/Lists/Motor%20Control%20Firmware%20and%20Software/ST%20MC%20Workbench%20%2b%20ST%20FOC%20library&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CE106710FFA6574FB92BFFEFCE2DD930&TopicsView=https://my.st.com/public/STe2ecommunities/motordriver_ics/Lists/Motor%2520Control%2520Firmware%2520and%2520Software/AllItems.aspx&currentviews=8]here an try don't duplicate the posts.

Ciao

Gigi