2008-11-09 08:59 PM
Low Power Mode problem
2011-05-17 03:50 AM
Hallo everybody,
First of all, my configuration :-D Ride7 version 7.14.0001 with RKit-ARM 1.13.0810 and STM32F103RBT6 daughterboard. Then, the problem ;-) I tried to use low power modes but I have some problems with this. When I use in my code any __WFI or __WFE istruction, after debugging and running the RUN led of RLink turns on but nothing happens - even if in the code I turn on some LEDs before using the __WFI istructions they are not turned on. In the new IDE version I am using, a message appears:''Lost communication with target.Terminating debug session''. I used also the PWR examples in STM FWLib, and others from STM website, but they all give me this problem. What could it be? Greeting.2011-05-17 03:50 AM
Nobody can help me?
2011-05-17 03:50 AM
You need to set a flag in the debug configuration registers to prevent the low power modes from shutting down the clock and/or power to the debug unit. I don't remember the name of the register, but it's in the debug section of the ref manual.
2011-05-17 03:50 AM
Thanks for the answer, your idea seems to me the right one but...I just tried the DBGMCU_Config function but I have the same problem. Here's the code:
int main(void) { RCC_Configuration(); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_BKP | RCC_APB1Periph_PWR,ENABLE); NVIC_Configuration(); GPIO_Configuration(); /*This should keep debugger connection during Sleep mode*/ DBGMCU_Config(DBGMCU_SLEEP, ENABLE); /* Config the EXTI to wake up from SLEEP Mode */ EXTI_Configuration(); /* Mode: SLEEP + Entry with WFI*/ __WFI(); while (1){} } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure PA.0 as input floating (EXTI Line0) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); } void EXTI_Configuration(void) { EXTI_InitTypeDef EXTI_InitStructure; GPIO_EXTILineConfig(GPIO_PortSourceGPIOA, GPIO_PinSource0); EXTI_ClearITPendingBit(EXTI_Line0); EXTI_InitStructure.EXTI_Line = EXTI_Line0; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); } void NVIC_Configuration(void) { NVIC_InitTypeDef NVIC_InitStructure; NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2); NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); } Really can't get why it doesn't work! [ This message was edited by: marcl on 10-11-2008 10:33 ]