cancel
Showing results for 
Search instead for 
Did you mean: 

Centre agligned pwm interrupt problem

markl2
Associate II
Posted on November 04, 2008 at 09:17

Centre agligned pwm interrupt problem

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
markl2
Associate II
Posted on May 17, 2011 at 12:50

Hi Guys,

I am trying to generate a interrput on the rising edge of center agligned pwm using TIM1_CCR4 but I keeping getting both rising & falling interrupts. Is possible to mask out the the falling edge interrupt?

TIM1_ARR=0xFFFF;

TIM1_CCR1=0x7FFF;

TIM1_CCR2=0x7FFF;

TIM1_CCER = TIM1_CCER_CC1E|TIM1_CCER_CC1NE|TIM1_CCER_CC2E|TIM1_CCER_CC2NE;

TIM1_BDTR = 0x02| TIM1_BDTR_OSSR|TIM1_BDTR_OSSI|TIM1_BDTR_AOE;

TIM1_EGR|= TIM1_EGR_UG;

TIM1_CR1 = TIM1_CR1_CEN|TIM1_CR1_ARPE| 2<

TIM1_CCMR1_OUTPUT_COMPARE_MODE = TIM1_MODE_PWM1<

TIM1_MODE_PWM1<

TIM1_CCR4=1;

TIM1_CCMR2_OUTPUT_COMPARE_MODE = TIM1_MODE_PWM2<

TIM1_CCER|= TIM1_CCER_CC4E;

TIM1_DIER = TIM1_DIER_CC4IE;

Irq_0_to_31_Set_Enable = 1<

thx