cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303K8 ADC Calibration phase problem

Jeck7778
Associate II
Posted on January 02, 2017 at 17:01

This is my CODE:

void ADC_t_init(void)

{

    ADC_InitTypeDef          ADC_InitStrc;

    ADC_CommonInitTypeDef     ADC_CmmInitStrc;

    /* Configure the ADC clock */

    RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div256);

    /* Enable ADC1 clock */

    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);

    /* Calibration procedure */

    ADC_StructInit(&ADC_InitStrc);

    ADC_Init(ADC1, &ADC_InitStrc);

    ADC_Cmd(ADC1, DISABLE);

    ADC_VoltageRegulatorCmd(ADC1, ENABLE);

    /* Insert delay equal to 10 µs */

    Delay(10);

    ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);

    ADC_StartCalibration(ADC1);

    while(ADC_GetCalibrationStatus(ADC1));

    calibration_value = ADC_GetCalibrationValue(ADC1);

    ADC_CmmInitStrc.ADC_Mode                 = ADC_Mode_Independent;

    ADC_CmmInitStrc.ADC_Clock                 = ADC_Clock_AsynClkMode;

    ADC_CmmInitStrc.ADC_DMAAccessMode         = ADC_DMAAccessMode_Disabled;

    ADC_CmmInitStrc.ADC_DMAMode             = ADC_DMAMode_OneShot;

    ADC_CmmInitStrc.ADC_TwoSamplingDelay     = 0;

    ADC_CommonInit(ADC1, &ADC_CmmInitStrc);

    ADC_InitStrc.ADC_ContinuousConvMode     = ADC_ContinuousConvMode_Enable;

    ADC_InitStrc.ADC_Resolution             = ADC_Resolution_12b;

    ADC_InitStrc.ADC_ExternalTrigConvEvent     = ADC_ExternalTrigConvEvent_0;

    ADC_InitStrc.ADC_ExternalTrigEventEdge     = ADC_ExternalTrigEventEdge_None;

    ADC_InitStrc.ADC_DataAlign                 = ADC_DataAlign_Right;

    ADC_InitStrc.ADC_OverrunMode             = ADC_OverrunMode_Disable;

    ADC_InitStrc.ADC_AutoInjMode             = ADC_AutoInjec_Disable;

    ADC_InitStrc.ADC_NbrOfRegChannel         = 1;

    ADC_Init(ADC1, &ADC_InitStrc);

    /* ADC1 Temperature sensor configuration */

    ADC_RegularChannelConfig(ADC1, ADC_Channel_TempSensor, 1, ADC_SampleTime_601Cycles5);

    /* Enable ADC1 */

    ADC_Cmd(ADC1, ENABLE);

    /* Enable temperature sensor */

    ADC_TempSensorCmd(ADC1,ENABLE);

    /* wait for ADRDY */

    while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));

    /* Start ADC1 Software Conversion */

    ADC_StartConversion(ADC1);

}

and the program not exit from:

while(ADC_GetCalibrationStatus(ADC1));

anyone know where is the problem?

thenks for help.

1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud GARSI
Lead II
Posted on January 10, 2017 at 10:32

Hi

Giacomo.Cimarelli

,

- Theline 'ADC_Cmd(ADC1, DISABLE);' will set the ADDIS bit (ADDIS=1).

Your ADC was never enabled before this line, so ADEN=0.

- On the reference manual, it's indicated that :

'Software is allowed to set ADDIS only when ADEN=1 and both ADSTART=0 and JADSTART=0

(which ensures that no conversion is ongoing)'

-> What you are trying to do is out of specification.

What you should do is to comment the line below: 'ADC_Cmd(ADC1, DISABLE);'

And your code will be executedconveniently.

Khouloud.

View solution in original post

4 REPLIES 4
Khouloud GARSI
Lead II
Posted on January 02, 2017 at 17:40

Hi

Giacomo.Cimarelli

,

You have disabled the

ADC1 peripheral using: ADC_Cmd(ADC1, DISABLE);

Try to enable it beforechecking the end of calibration.

If this solves your issue, please click on correct

🙂

.

Happy new year .

Khouloud.

Posted on January 03, 2017 at 00:33

Hi

Khouloud G

.

On the ST Reference Manual is written:

The calibration is then initiated by software by setting bit ADCAL=1. Calibration can only be

initiated when the ADC is disabled (when ADEN=0). ADCAL bit stays at 1 during all the

calibration sequence. It is then cleared by hardware as soon the calibration completes. At

this time, the associated calibration factor is stored internally in the analog ADC and also in

the bits CALFACT_S[6:0] or CALFACT_D[6:0] of ADCx_CALFACT register (depending on

single-ended or differential input calibration)

For the calibration need kept ADC disabled right?

I have try to enabling it but not work.

Khouloud GARSI
Lead II
Posted on January 10, 2017 at 10:32

Hi

Giacomo.Cimarelli

,

- Theline 'ADC_Cmd(ADC1, DISABLE);' will set the ADDIS bit (ADDIS=1).

Your ADC was never enabled before this line, so ADEN=0.

- On the reference manual, it's indicated that :

'Software is allowed to set ADDIS only when ADEN=1 and both ADSTART=0 and JADSTART=0

(which ensures that no conversion is ongoing)'

-> What you are trying to do is out of specification.

What you should do is to comment the line below: 'ADC_Cmd(ADC1, DISABLE);'

And your code will be executedconveniently.

Khouloud.

Posted on January 10, 2017 at 12:56

Thenks for the help now work!