Skip to main content
tderensis
Associate
October 19, 2015
Question

STM32F0 Unique ID Location

  • October 19, 2015
  • 2 replies
  • 1957 views
Posted on October 19, 2015 at 21:18

What is the starting address of the 96-bit Unique ID on the STM32F030 processors? I cannot find this information anywhere in the reference manual or datasheet. Is this guaranteed to exist on the F0 series?

#stm32f0 #unique-id
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
October 19, 2015
Posted on October 19, 2015 at 21:44

Some F0 parts do, the page for the

http://www.st.com/web/en/catalog/mmc/SC1169/SS1574/LN1826/PF258968

doesn't claim it has one, whereas the

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN1447/PF253344?sc=internet/mcu/product/253344.jsp

does. Bottom of the ''Key Features'' list.

The absence in

http://www.st.com/web/en/resource/technical/document/reference_manual/DM00091010.pdf

Chap 27, also would seem to confirm that it's not present/supported in your chosen chip. Would appear to be a purposeful omission.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Technical Moderator
October 20, 2015
Posted on October 20, 2015 at 18:08

Hi derensis.thomas,

I confirm that the Unique ID isn't available for STM32F030x4/6/8/C and STM32F070x6/B (the ones covered by RM0360).

Please note that STM32F050 devices were renamed to STM32F031 (RM0091). Tha's why it supports the Unique ID feature.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.