cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect SMPS to control TRIAC with negative triggering circuit?

Nazmul Hasan
Associate III

Posted on August 14, 2017 at 05:21

Hello

I want to control ST's snubberless triac (T435-800) directly from MCU (STM32F0). According to AN3168 (article 2.4), I've to connect AC main (220V, 50Hz) supply with the control circuit's Vdd. In AN392, I found the same that illustrate triac control with negative power supply, but uses capacitive dropper. Actually, I didn't understand what's going on there after connecting AC main with +5V DC. Why not the control circuit get affected by the AC main? All I want to do the same as AN392, but wants to use SMPS (STEVAL-ISA010V1, based on Viper16). Is it okay to connect SMPS's positive terminal directly to AC main? or Do I need anything else such as diode clipper?

Thanking you.

#triac #smps

1 ACCEPTED SOLUTION

Accepted Solutions
Nazmul Hasan
Associate III
Posted on August 14, 2017 at 20:31

All right, AN4564 explained all I need.

0690X0000060417QAA.jpg

View solution in original post

1 REPLY 1
Nazmul Hasan
Associate III
Posted on August 14, 2017 at 20:31

All right, AN4564 explained all I need.

0690X0000060417QAA.jpg