cancel
Showing results for 
Search instead for 
Did you mean: 

ethernet can send data, but can not receive data

janesnoopy
Associate
Posted on November 21, 2006 at 10:46

ethernet can send data, but can not receive data

2 REPLIES 2
janesnoopy
Associate
Posted on May 17, 2011 at 09:34

HI.

I debug the demo STR91x_webserver_v1_1 in my board. but i found the board could not receive the data from the PC, but can send data to PC. I found the RX START REGISTER.DMA_EN always be set '1', and the RX Packet status VALID BIT is set '1' also. so i don't know why the DMA Could not be reset the VALID bit. Thank you.

anis
Associate II
Posted on May 17, 2011 at 09:34

Hi Janesnoopy,

From what I understand, you are not able to load the webpage, when typing the webserver address 192.168.0.8 in your browser, is this correct?