cancel
Showing results for 
Search instead for 
Did you mean: 

ST, all but userfriendly

woutervddn
Associate
Posted on November 12, 2010 at 18:30

hi all,

first of, I just got my STM32VL Discovery. And it looks nice!

I took it out, pluged it in and an played with the buttons..

NICE!

Next step: (5 on the cardboard btw)

to study or modify the DISCOVER project related to this simple demo,

visit www.st.com/stm32-discovery and follow the tutorial.

Nice try but a 404 is given..

After some google search I decided to download Atollic.

I find the st tutorial and think I'm all set.

Guess again.. the tutorial says I have to go to the stm32vl_discovery directory..

But I can't find it (how could I, I didn't even downloaded something from st).

Anyways, my google search starts again, and by wonder I stumble upon the an3268 package. I hate to say it, but this is sh*t, how could I knew this? I never, ever found a download location. I didn't even got the hint that I had to download something..

But I'm set, atleast I think..

in the next step I need to add a variable path.. It points to a FIRMWARE folder,.. NICE, but where the hell is it located? I couldn't find it, so I suppose it's another download link... 

But where in earth can I find it? One thing is certain, NOT in the tutorial..

Wouter Vandenneucker

PS: can someone pls give me that link.. it's kind of frustrating..

#firmware #stm32vl #package #tutorial
10 REPLIES 10
Posted on November 12, 2010 at 23:45

The site is in transition

Here is the new discovery page, files under Design Support tab

http://www.st.com/internet/evalboard/product/250863.jsp

http://www.st.com/internet/evalboard/product/250863.jsp

Firmware source/libraries

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3268.zip

http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3268.zip

These need to be unzipped in a suitable place, with Keil under Examples\ST worked for me.

I wouldn't touch Atollic Lite, it doesn't support project files, and building stuff for the VL board was a battle. Keil was easier, but embedded stuff generally assumes you can use, or are familiar, with the tools.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist III
Posted on November 13, 2010 at 08:04

''The site is in transition''

From something that was usable to something that is not!

:-(

Note that the 

http://www.st.com/stm32-discovery

URL has now been fixed.

But I'm sure you'll not be the only one to be seriously frustrated by this gross stupidity on ST's part! Especially as it coincides with the launch of two design contests (that I know of)!!

See the following thread for discussion about the dreadful new website: 

[DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General comments and feedback/Website Wrecked!&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0

alwebbox
Associate
Posted on November 16, 2010 at 07:17

Andrew Neil
Evangelist III
Posted on November 16, 2010 at 09:13

''I wouldn't touch Atollic Lite, it doesn't support project files''

 

It also completely prevents you from using printf!

That's not just that it doesn't come with a complete implementation, so you have to write your own - they have specifically disabled the facilities needed to allow you to use it at all!!

''I selected the Atollic option based on the fact that it has no code size restrictions and therefore seemed to be the most capable''

See above!

Andrew Neil
Evangelist III
Posted on November 16, 2010 at 21:56

(deleted by me)

alwebbox
Associate
Posted on November 17, 2010 at 04:48

''It also completely prevents you from using printf!''

 

 

Maybe that's what they mean in the feature comparison guide?

I/O redirection of runtime library - not in Lite version
Andrew Neil
Evangelist III
Posted on November 17, 2010 at 08:02

''It also completely prevents you from using printf!''

 

 

Maybe that's what they mean in the feature comparison guide?

 

I/O redirection of runtime library - not in Lite version

 

 

Yes - I think so.
qili
Associate II
Posted on November 20, 2010 at 12:50

I have to say that my first impression with the redesigned st.com site that it must have been designed by nxp or one of st's competitors.

it is so bad and so hard to use that there is no other explanation.

Andrew Neil
Evangelist III
Posted on November 20, 2010 at 20:32

Please keep comments about the new website in the specific thread about it:

[DEAD LINK /public/STe2ecommunities/e2efeedback/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked%21&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0&currentviews=292]https://my.st.com/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Flat.aspx?RootFolder=/public/STe2ecommunities/e2esupport/Lists/General%20comments%20and%20feedback/Website%20Wrecked!&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800012C78846220B4D4494A7455BB1CA77C0&currentviews=292

That way ST can see all the posts together - rather than have them ''hidden'' in other threads.