cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F10x DSP library

animeshmaurya
Associate
Posted on January 13, 2011 at 08:24

Hi everyone,

I was wondering if anyone has used STM32F10x DSP library with the discovery board?

Does the library support STM32VL-Discovery?

Thanks

1 REPLY 1
Posted on January 13, 2011 at 20:58

Does the library support STM32VL-Discovery?

Why wouldn't it, and what would preclude you from trying it?

The processor uses the same Cortex M3 core the code is compiled/assembled for. It will run slower than on a 72 MHz variant, as the VL is limited to 24 MHz operation. But you are talking math routines, not peripheral locked code.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..