Skip to main content
waclawek.jan
Super User
May 17, 2017
Solved

Does SPI in slave mode threestate MISO on inactive NSS, or not?

  • May 17, 2017
  • 1 reply
  • 1240 views
Posted on May 17, 2017 at 23:22

This is a followup to

https://community.st.com/thread/40921-multi-slave-spi-using-stm32f7s&sharpcomment-157367

.

RM0385, requests MISO being set to open-drain when multiple slaves are connected. This indicates, that NSS set to the inactive state *does not* threestate MISO in STM32 SPI set to slave, as is the custom with SPI. This makes using multiple STM32 SPI slaves not practical.

0690X00000606sZQAQ.png

Other than this, I could not find any indication of MISO behaviour in this regard in the RM.

I also went to the respective datasheet and the graph indicates that MISO *does* threestate when NSS goes inactive:

0690X000006072SQAQ.png

The STM32F40x DS, in the same table, for the same parameter, the footnote clearly states that MISO is to be threestated (put to Hi-Z)

0690X00000606v6QAA.png

ST, please comment.

Jan Waclawek

null
    This topic has been closed for replies.
    Best answer by Petr Sladecek
    Posted on May 18, 2017 at 13:03

    Hello,

    MISO signal output is under standard chip select control of NSS input when the SPI slave is enabled and configured at HW NSS mode with NSS output disabled (SPE=1, SSM=0 nad SSOE=0). This allows multi-slave star topology communication.

    Best regards,

    Petr

    1 reply

    Petr Sladecek
    Petr SladecekBest answer
    ST Employee
    May 18, 2017
    Posted on May 18, 2017 at 13:03

    Hello,

    MISO signal output is under standard chip select control of NSS input when the SPI slave is enabled and configured at HW NSS mode with NSS output disabled (SPE=1, SSM=0 nad SSOE=0). This allows multi-slave star topology communication.

    Best regards,

    Petr