2015-12-21 2:19 AM
Hello to all,
I am currently converting my Code from ST Periperal Lib to Cube which is a hell of a work because EVERYTHING has changed. The function names, the structures, the constants. I am using a STM32F2xx. I have to enable the backup voltage regulator. In STPerLib this was done with PWR_BackupRegulatorCmd(ENABLE); The bit was defined there nicely with bit banding. In cube I miss this function. How can it be done with cube? Thanks a lot Andy2015-12-21 4:58 AM
Hi Andy,
To enable the Backup Regulator you may use the function declared in the stm32f2xx_hal_pwr_ex.c file: HAL_StatusTypeDef HAL_PWREx_EnableBkUpReg() -Syrine-2015-12-21 5:42 AM
Hello Syrine,
thanks a lot for your quick answer! The pwr-cube files were not linked to my project thats why I did not find it. Please one more question to make my work easier: I have a working project with ST Per Lib. In order to convert it to Cube sometimes I have to dive into the appropriate function in STPerLib, copy some destinctive cpu register or constant names and search for these strings throughout my new project with cube. Thus I can find the corresponding cube function. This a strenuous work though. The only doc for cube I found in UM1940 user manual which is a pdf only. In contrast to this the doc for STMPerLib was a nice *.chm Help-File: http://www.st.com/web/en/catalog/tools/PF257898# It has a lot of text links and is much more conveniant. I would be happy if you can post me a link for the same help file for cube STM32F2xx. But first of all I wish you a happy christmas with a good time and less bits and bytes! Andy2015-12-21 6:36 AM
Hi Andy,
You can find the *.chm file for STM32F2xx HAL Drivers underSTM32Cube_FW_F2_V1.3.0\Drivers\STM32F2xx_HAL_Driver\Merry Christmas :)-Syrine-
2015-12-21 8:46 AM
Hi Syrine,
thank you for your hint with the help file. However I downloaded the STM32Cube_FW_F2_V1.3.0Within STM32Cube_FW_F2_V1.3.0\Drivers\STM32F2xx_HAL_Driver\
I found 2 files, each only about 7MB size:
STM32F215xx_User_Manual.chm and
STM32F217xx_User_Manual.chm
When I open them they show only the contents structure in the left column, but nothing in the main screen.
The STPerLib chm file on the other side is 17MB!
So I think these 2 files are somehow not complete.
Thanks again for your kind help
Andy